Search
RSLinx Classic Help
DDE/OPC communication event errors
Troubleshooting
:6Ah error in the DDE/OPC Communications Event Log
A DDE/OPC Client has caused an exception to occur in the DDE/OPC subsystem
CIP IOI Syntax Error, tag may not exist
CIP Messaging Error: A message timed out waiting for a response
Connection dropped while trying to read a ControlLogix Optimized Packet
ControlLogix attempted to read a ControlLogix Optimized packet
ControlLogix connection 602191 got disconnected
ControlLogix Optimized packet being reinitialized
ControlLogix optimized packet response while in Initialized state
Could not find TOpt for ControlLogix Optimized packet
Data read for a ControlLogix Optimized packet with no data returned
Error adding a ControlLogix Optimized item
Error trying to add or remove ControlLogix Optimized items
Failed to establish communication with controller
This is an undefined topic. Verify the topic is in the current project
This item does not exist in the processor
What do I need to configure when creating a remote OPC connection?
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal