Error trying to add or remove ControlLogix Optimized items
Error trying to add or remove ControlLogix Optimized (0 of 9) items from the processor 204
Possible solution
Error code 204 indicates that this is a timeout trying to communicate with the controller. Possible solutions are to allow more processing time in the controller or to reduce network traffic.
Provide Feedback