Error adding a ControlLogix Optimized item
Error adding a ControlLogix Optimized item [10500ce, 0] in the ControlLogix optimized packet[e] for item 'Program:FD1360_Ingredient_Mixing.P1360_403ST[1]'.
Possible solution
Depending on the ControlLogix firmware, this could be a firmware bug where the first time I try to add it, it fails, and the next time it passes.
Provide Feedback