ControlLogix Optimized packet being reinitialized
ControlLogix Optimized packet being reinitialized 45c0078, connection 602191, packet's read connection 0
Possible solution
This is often paired with the
ControlLogix connection 602191 got disconnected
event when communicating to a heavily loaded ControlLogix processor. This means RSLinx Classic was able to continue data collection from the ControlLogix processor. 45c0078 is the ID of the ControlLogix Optimized packet, and 602191 is the ID of the connection.Provide Feedback