A DDE/OPC Client has caused an exception to occur in the DDE/OPC subsystem
Possible solution
Either an OPC or DDE client is requesting invalid ControlLogix tags or there is an internal problem with data handling in the OPC/DDE application. This error also gets logged into the Windows event log. Verify through your OPC/DDE applications that all requested tags actually exist in the ControlLogix processor.
Provide Feedback