User accounts and user groups
Symptoms of problems related to managing user and user group accounts:
- Cannot disable or delete a particular user account
- Cannot enable a deleted user account
- Cannot add Windows-linked accounts
- An enabled Windows-linked account shows as disabled
- Cannot add users or groups
- Recreating deleted accounts does not restore permissions
- Windows users are gaining access without having accounts
- Unable to grant full access to the network directory
Provide Feedback