I cannot disable or delete a particular user account
To prevent inadvertent lock out of the
FactoryTalk Directory
, the last user account that is a member of the Administrators group cannot be deleted.If all existing Administrator user accounts must be deleted, create a new user account and assign it to the Administrators group. Then all of the previous account can be deleted.
IMPORTANT:
Security settings are completely separate in the Network Directory and Local Directory. Changes you make to the security settings in the Network Directory do not affect the Local Directory and vice versa. If using both a Network and a Local directory, set up security in each directory separately.
Provide Feedback