Add a FactoryTalk user account
To create a user account that is separate from a user's
Windows
account, add a FactoryTalk Directory
account. FactoryTalk Directory
accounts are managed by the FactoryTalk
Administrator and specify the account's identity, account policy, and group membership independent of the Windows
account settings. Prerequisites
Obtain these permissions for the
Users
folder in the Explorer
window:- Common > Create Children
- Common > List Children
- Common > Read
To add a user account
- InExplorer, expandSystem>Users.
- Right-click theUsersfolder, point toNew, and then selectUser.
- InNew, type a short name for the user inFactoryTalkUserUser Name, and the full name of the user inFull name.
- (optional) InDescription, record information about the user, such as the user's position or phone number.
- (optional) InE-mail,add a single e-mail address. SomeFactoryTalkproducts may send messages to this e-mail address.
- InLogin methodselect how the user logs on toFactoryTalk.
- Password. The user types the user name and password to logon.
- Badge only. The user taps the badge on the card reader to logon.
- Password and Badge. The user taps the badge on the card reader and types the username and password to logon.Badge logon is not supported on remote clients connecting via Remote Desktop Services. To log on using an RFID badge, connect an rf IDEAS card reader to the computer hosting theFactoryTalk Services Platform.
- If a password method was selected, inPassword, type a password for the user account.Password Policy SettingsinSecurity Policy Propertiesdetermine the requirements for a valid password.TIP:The maximum password length is 64 characters. However, the dialog box only displays 35 characters. Characters not shown are still included in the password.
- InConfirm, type the same password entered in the previous step.
- (optional) If a password method was selected for login, select the user's password validity settings:
- User must change password at next logon
- Select to force the user to change the account password at next system log on.
- Clear to allow the user to keep the same password.
- User cannot change password
- Select to prevent the user from changing the account password.
- Clear to allow the user to change the account password.
- Password never expires
- Select to allow the user to continue using the same password indefinitely.
- Clear to require that the user change the account password at intervals specified by the security policyPassword Policy Settings.
- InBadge IDtype the identification number of the badge assigned to the user account.SelectScanand then tap the badge on the card reader to obtain theBadge IDvalue from the badge.
- SelectOKto add the user to theFactoryTalk Directory.
Provide Feedback