Delete a user account
Delete a user account to permanently remove the account from the
FactoryTalk Directory
. To prevent inadvertently locking an account out of the FactoryTalk Directory
, do not delete the last user account that is a member of the Administrators group. To delete a user account from both a network directory and a local directory, delete the account from one directory, log off that directory, log on to the second directory, and then delete the account in the second directory.
To temporarily prevent a user from logging on to
FactoryTalk
, disable the FactoryTalk
user account.Prerequisites
Deleting a user account that is a member of a user group requires these permissions:
- Common > Delete
- Common > List Children
- Common > Read
- Common > Write
Deleting a user account that is not a member of a user group requires these permissions:
- Common > Delete
- Common > List Children
- Common > Read
To delete a user account
- InFactoryTalk Administration ConsoleExplorer, expandSystem>Users, right-click the user account, and then selectDelete.You can also use Historical Usage to delete a user account.TIP:You can only create an account using the name of a deleted account if the security policyKeep record of deleted accountsis disabled. You must still recreate the security settings of the user accounts.
Provide Feedback