Add and remove permission sets
Starting from version 2.80,
FactoryTalk Services Platform
supports Permission Sets that identify a set of actions that are allowed or denied for one or more user groups or computer groups. Use permission sets in Studio 5000 Logix Designer version 28.00 or later to apply the same permissions to multiple ControlLogix controllers or project components.
TIP:
We recommend that you use Permission Sets to improve the efficiency of the FactoryTalk Directory cache synchronization.
Provide Feedback