Delete a permission set

Delete a permission set when that set of permissions is no longer needed to apply to multiple controllers or project components in a
Logix Designer
application.
Prerequisites
Before deleting a permission set, obtain the following security permissions for the
Permission sets
folder:
  • Common > Read
  • Common > List Children
  • Common > Delete
To delete a permission set
  • Expand
    System
    >
    Permission Sets,
    right-click the permission set, and select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal