New Permission Set

Permission sets identify a set of actions that are allowed or denied for one or more user groups or computer groups. Use permission sets to apply the same permissions to multiple controllers or project components.
Use
New Permission Set
to create a permission set.
Setting
Description
Name
Type a descriptive name to identify the permission set.
Description
Type an optional description of the permission set.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal