Secure a FactoryTalk system

FactoryTalk Security
improves the security of the automation system by limiting access to those with a legitimate need.
FactoryTalk Security
authenticates the identities of users and authorizes user requests to access a
FactoryTalk
system against a set of defined user accounts and access permissions held in the
FactoryTalk
network directory or
FactoryTalk
local directory.
Resources in a
FactoryTalk
system that can be secured include:
Combine these
FactoryTalk Security
features to build an ideal security solution:
The principle of
inheritance
determines how access permissions are set. For example, if assigning security to an area in an application, all of the objects in the area inherit the security settings of the area. Override this behavior by setting up security for one or more objects inside the area.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal