Audit security
Specify what security-related information is recorded while using
FactoryTalk Security
. Audit policies include whether modifications to control system components are tracked, and whether access grants, denies, or both are audited. Audit messages are sent to FactoryTalk Diagnostics
. Messages are viewed using the FactoryTalk Diagnostics
Viewer. Set audit policies to:
Provide Feedback