General Permission Set Properties

Permission sets identify a set of actions that are allowed or denied for one or more user groups or computer groups. Use permission sets to apply the same permissions to multiple controllers or project components. For more information about how to use permission sets with
Logix Designer
, see the
FactoryTalk System Configuration Guide
.
Use
General Permission Set Properties
to modify a permission set. The name of the permission set cannot be changed.
Setting
Description
Description
Type an optional description of the permission set.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal