Commands in Project Organizer
Use
Project Organizer
to open and edit additional device configuration options. Micro800
controllers and drives are available in Project Organizer
.Commands available for Micro800 controllers
Right-click and select | To |
|---|---|
Connect | |
Disconnect | |
Clean | |
Fault | Open <controller-name>:Fault to view and clear controller faults. |
Import > Global variables | |
Import > Data types | |
Export > Global variables | |
Export > Data types | |
Delete | Remove the Micro800 controller from Project Organizer . You can also use the Delete key. |
Data protection | Open Data protection to add or remove variables from a list of the protected variables. |
Memory module backup and restore | Open Memory module backup and restore to configure the relevant settings and start the backup or restore process. |
Commands available for Class 1 devices, plug-in modules, and expansion modules
Right-click and select | To |
|---|---|
Delete | Remove a drive, plug-in module, or expansion module from Project Organizer . You can also use the Delete key to remove the device. |
Provide Feedback