Fault diagnostics
Use the
<controller-name>: Fault
view to:- View information on any faults that occurred.
- Retrieve a detailed fault log or core dump file from the controller.
- Clear a fault.
The
<controller-name>: Fault
view shows the last seven recoverable and the last seven non-recoverable faults with:- The fault code
- Fault location and the link if available
- A description of the fault
The
<controller-name>: Fault
view is available by selecting the Fault
button from the Connection
pane when the controller is in Remote run
mode.Controller Fault view

Item | Description |
|---|---|
Clear fault | Deletes the faults and fault logs from the controller. |
Get fault log | Retrieves the detailed faults and fault logs from the controller. The information can be used when seeking technical support. By default, the fault log is saved as a TXT file in the Downloads folder. You can customize the path as needed. |
Get core dump fault log | Retrieves the core dump of Micro800 controller to a Bin file, which you can send to the Rockwell Automation engineering team for troubleshooting and debugging.By default, the core dump is stored with the name Controller_Core_Dump_mm_dd_yyyy_hh_min_sec.bin in the Downloads folder.You can customize the path as needed. The size limit for the core dump is 8,192 bytes. Upgrading the firmware clears the core dump. |
Recoverable/Non-recoverable Fault | Displays two types of faults:
|
Index | Displays the sequential number of the faults. The index number 1 indicates the last fault. |
Fault Code | Displays the fault code in hexadecimal. |
Location | Displays the fault location and provides a link to the program, if available. |
Description | Displays the information about the fault. |
Provide Feedback