Download a controller configuration to a controller
Use
Download device
to download a project from FactoryTalk Design Workbench
to a Micro800
controller for running and testing. The project can contain programs, variables, and controller configurations.When downloading the project, if the controller revision doesn't match the one defined in the
FactoryTalk Design Workbench
project, the Update and download
dialog opens. Use the dialog to update the controller revision, and then download the project again.When the download begins,
FactoryTalk Design Workbench
performs the following tasks:- Builds any unbuilt programs.
- Compares the configuration of the connected controller with the project configuration.
- Downloads the project, programs, variables, and controller configuration to the controller.
If an error occurs when performing any of the tasks, the download is canceled, and the controller remains unchanged.
If the initial value for the variable is set to the default value for the data type, such as 0, 0.0, D#1970-01-01,
FactoryTalk Design Workbench
initializes the variable with its value.
TIP:
When initializing variables with project values, the following conditions apply:
- Variables with aDirectionofVarInputcannot be downloaded.
- Variables with anAttributeofReadorNo Accesscannot be downloaded.
- Complex variables, such as structures and arrays that contain members with initial values, cannot be downloaded.
- Variables with both a value and an initial value will be initialized with their initial value.
Prerequisites
- Set the connection path for the controller.
- The catalog number of the controller in the current project matches the one you're downloading to.
To download a controller configuration to a controller
- Select
to open Online center. - From theDevicelist, select the controller, and then selectDownload.
- InDownload device, selectOK.
- Use theOutputpane to view the result.
- (optional) Resolve any errors, and then download the configuration again.
Provide Feedback