Project Organizer
Project Organizer
displays the devices and program elements of the project in an organized tree view. Use Project Organizer
to open additional device configuration workspaces and manage program elements. If no device is added, use the New device or Discover Device button to add one. Elements displayed in Project Organizer
vary with the added device.For projects that contain a
Micro800
controller, Project Organizer
displays the following items that are associated with the controller:- Global variables
- Assets, including user-defined functions, user-defined function blocks, and user-defined data types
- I/O configurations
Project Organizer

Item | Description |
|---|---|
![]() | Opens Add device to add devices to the project. |
![]() | Deletes the selected device from the project. |
![]() | Opens Select Device to view a list of devices that are connected to the computer. |
Provide Feedback