Discover and add a controller connected to a computer
Use
Select device
to view and add the devices connected to a computer. You can use the function to:- Replace the existing controller in the controller project with the discovered one.
- Add a controller and its controller project to an empty project.
Prerequisites
- The controller is offline.
To discover and add a controller connected to a computer
- OpenSelect deviceby doing one of the following:
- InProject Organizer, select
. - InProject Organizer, selectDiscover device.
- InProject Organizer, right-click a blank space, and then selectDiscover device.
- Open Add device, and then selectDiscover device.
- InSelect device, turn on auto-browsing or refresh the browser to display all the devices recognized byFactoryTalk Design Workbenchthat are connected to your computer through an enabled communication port.
- Select the device, and then selectOK.The device is added to the project andProject Organizer.
- (optional) If you've already added a controller to the project and are selecting another controller fromSelect device,Discover controlleropens, asking if you want to replace the existing controller with the selected one. SelectReplace.
Provide Feedback