Secure a controller with a password
Create a password for a
Micro800
controller to prevent unauthorized access to the configuration and programming in the controller.When a controller is configured with a password, you must enter the password before doing any of the following:
IMPORTANT:
If the existing password is forgotten or lost, it cannot be recovered, changed, or cleared. If a controller fault occurs during password configuration, restart the controller and reconfigure the password.
Prerequisites
- The controller is inRemote programmode.
To secure a controller with a password
- OpenChange password for <controller-name>by doing one of the following:
- InConnection, selectSecure, and then selectSet password.
- InProject Organizer, right-click the controller, and then select .
- InProject Organizer, select the controller, and then from the menu bar, select .
- InChange password for <project-name>, enter a password. Passwords must be 8 to 64 characters long, which can include letters, numbers, spaces, and any keyboard symbols.
- InConfirmation, enter the exact password again.
- (optional) To view the password, select
. - SelectOK.
Provide Feedback