Clear the controller password
Before clearing the password for a
Micro800
controller, you must have the current password.Prerequisites
- The controller is inRemote programmode.
To clear the controller password
- OpenClear password for <controller-name>by doing one of the following:
- InConnection, selectSecure, and then selectClear password.
- InProject Organizer, right-click the controller node, and then select .
- InProject Organizer, select the controller, and then from the menu bar, select .
- InClear password for <controller-name>, enter the password.To view the password, select
. - SelectOK.
Provide Feedback