Connect to a password-protected controller
You must have the password before connecting to a password-protected controller.
Micro800
controllers allow the connection of one configuration tool at a time. You cannot connect to the controller when:- The controller is locked by another user.
- The type of the selected controller does not match the one defined in the opened project.
To connect to a password-protected controller
- From the menu bar, select
to open Online center. - InOnline center, do one of the following:
- In thePathcolumn, enter the controller connection path.
- Select
to open Select device, find and select the controller, and then selectOK.
- Connect to the controller by doing one of the following:
- InConnection, turn on the toggle beside theMicro800controller.
- InProject Organizer, right-click the controller, and then selectConnect.
- InEnter password, enter the controller password, and then selectOK.IMPORTANT:The controller will enter the locked-out state after a total of 11 or more unsuccessful password attempts, whether consecutive or spread out over time. In the locked-out state, the following conditions apply:
- A subsequent attempt with the correct password will only succeed after 300 seconds (locked-out duration).
- If you do not make subsequent attempts, the controller will automatically reset the unsuccessful sign-in count and exit the locked-out state after one day (auto unlock duration).
Provide Feedback