Change the controller password
Before changing the controller password, you must have the current password.
IMPORTANT:
If the existing password is forgotten or lost, there is no way to recover or change the password.
We recommend changing the controller password periodically to protect the programs and functions in the controller.
Passwords must be 8 to 64 characters long, which can include letters, numbers, spaces, and any keyboard symbols.
Prerequisites
- The controller is inRemote programmode.
To change the controller password
- OpenChange password for <controller-name>by doing one of the following:
- InConnection, selectSecure, and then selectChange password.
- InProject Organizer, right-click the controller, and then select .
- InProject Organizer, select the controller, and then from the menu bar, select .
- InChange password for <controller-name>, do the following:
- Enter your current password.
- Enter your new password.
- Enter your new password again to confirm it.
To view the password, select
. - SelectOK.
Provide Feedback