Upload a controller configuration from a controller
Use
Upload device
to upload a project containing programs, variables, and controller configurations from a Micro800
controller to FactoryTalk Design Workbench
. All project programs, variables, and controller configurations are overwritten after an upload. Once the project is uploaded to FactoryTalk Design Workbench
, you can edit the controller project, and then download it back to the controller.Prerequisites
- Set the connection path for the controller.
- The catalog number of the controller in the current project matches the one you're uploading from.
To upload a controller configuration from a controller
- Select
to open Online center. - InOnline center, from theDevicelist, select the controller, and then selectUpload.
- InUpload device, selectOK.TIP: COP instruction blocks do not upload values for Src and Dest variables. Other instruction blocks and variables are not affected.
- Use theOutputpane to view the result.
- If there are errors, resolve them, and then upload again.
Provide Feedback