Data protection
Use
Data protection
to create multiple user-defined global variables that retain their values when:- Restoring a controller project from a memory module (available for L20E, L50E, and L70E controllers).
- Downloading a project, programs, variables, and controller configurations to aMicro800controller (available for L20E, L50E, and L70E controllers).
In
FactoryTalk Design Workbench
, the variables that are defined for data protection retain their values if the project stored in the memory module and the current controller project meet the following criteria:- The variable name, data type, and number of bytes are defined the same in both projects.
- The arrays and array dimensions are defined the same in both projects.
- The variable is configured with data protection in both projects.
Column | Description |
|---|---|
No. | Displays the index number of the variable. Deleting a variable causes the indexes of all the subsequent variables to decrement by one. Up to 60 global variables are supported for data protection. |
Variable Name | Displays the user-defined variable name. |
Data Type | Displays the data type of the global variable. Supported data types are: BOOL, BYTE, DATE, DINT, DWORD, INT, LINT, LREAL, LWORD, REAL, SINT, TIME, UDINT, UINT, ULINT, USINT, WORD, and USER ARRAYS. |
Provide Feedback