Create local messages
Use the Local Messages editor to create messages that will appear in a local message display, and to specify their trigger values. You can define up to 10,000 messages in each message file.
To create local messages:
- InFactoryTalk View Studio, in theExplorerwindow, double-click theGraphicsfolder to open it, if necessary, and then double-click theLocal Messagesicon.
- In theLocal Messageseditor, enter a trigger value and its message.TIP:When you type the first value, a new line is created in the spreadsheet.When you right-click in a row, a context help that contains editing commands, opens.
- Repeat this for as many triggers as are required.TIP:To sort messages, highlight the rows to sort, right-click in any row, and then selectSort. The messages are sorted by trigger value.
- ClickClose, to name and save the messages file.
Provide Feedback