Local Messages editor

The following table shows options in the
Local Messages
editor.
Options
Description
Trigger value
Type an integer trigger value. You can use positive and negative numbers. Do not use 0. Trigger values do not need to be contiguous, but they must be unique for each message. For example, you could use trigger values of 1, 2, and 3, or values of 10, 20, and 30. The trigger value cannot be blank.
Message
Type the message, up to 256 characters long. You can use the new line character, \n, to specify that the message continues onto the next line after the character. To add a string to the message, right-click the Message column and then click Edit String to open the String Edit dialog box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal