Set up a connection for a local message display

Use the
Connections
tab to set up a connection for a local message display object.
To set up a connection for a local message display:
  1. In a display, double-click the object to open the L
    ocal Message Display Properties
    dialog box.
  2. Click the
    Connections
    tab.
  3. Assign a tag or expression to the
    Value
    connection:
    • Value
    • Message File, if you want to use a variable message file
    • Echo Message, if you want to write the triggered message to a tag
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal