Local Message Display Properties - Connections tab
The following table shows the options in the
Connections
tab of Local Message Display Properties
.Options | Description |
|---|---|
Value | Assign a tag or expression to this connection. It will be monitored for values that trigger messages. |
Message File | Assign a string tag or expression that will be used as the message file. To use this option, select the Use variable message file check box on the General tab. |
Echo Message | Assign a tag that the triggered message will be written to. To use this option, select the Use echo message check box on the General tab. |
The following table shows the columns in the
Connections
tab.Options | Description |
|---|---|
Name | This column shows the name of the connection. |
Value update direction | This column shows an arrow to indicate which way data can flow between the connection and the data source. tag or expression updates the data source (write connection) data source updates the tag or expression (read connection) tag or expression updates the data source and data source updates the tag or expression (read-write connection) |
Tag/Expression | Type the tag name or expression associated with the connection. If a tag or expression has already been selected, it is displayed here. |
Tag button (...) | Click this button to open the Tag Browser and choose a tag instead of typing the tag name in the Tag/Expression column. |
Exprn button (...) | Click this button to open the Expression editor and create an expression instead of typing the expression in the Tag/Expression column. |
Provide Feedback
tag or expression updates the data source (write connection)
data source updates the tag or expression (read connection)
tag or expression updates the data source and data source updates the tag or expression (read-write connection)