Configure general properties of a local message display
You can set up how the local message display looks at runtime.
To configure general properties of a local message display:
- In theLocal Message Display Propertiesdialog box, in theGeneraltab, specify the following properties if needed:
- General appearance
- Message file to use with the display
- Whether to use echo messageTIP:You can use the symbol for a new line, \n, in your messages in the message file to control where a message begins a new line. Or you can select theWord wrapoption, to let the application begin a new line when the next word won’t fit on the current line.
Provide Feedback