Fallos de movimiento

El siguiente diagrama muestra la jerarquía de los fallos relacionados con el eje: Fallos de eje y Fallos de grupo de movimiento, relacionados con la aplicación Logix Designer. Las abreviaturas de los tipos de eje (axis) a los que se aplica el fallo se muestran en paréntesis junto a cada fallo.
Símbolo
Tipo de eje (axis)
C
AXIS_CONSUMED
CD
AXIS_CIP_DRIVE
S
AXIS_SERVO
SD
AXIS_SERVO_DRIVE
V
AXIS_VIRTUAL
AxisFault (C, S, SD, V, CD)
GroupFault (C, S, SD, V, CD)
up arrow
up arrow
GroupOverlapFault (C, S, SD, V, CD)
motion faults line arrows
PhysicalAxisFault (C, S, SD, V, CD)
ModuleFault (C, S, SD, V, CD)
ConfigFault (C, S, SD, V, CD)
motion faults line up arrow
up arrow
up arrow
CIPAxisFaults (CD)
ModuleFaults (S, SD, CD)
motion faults line up arrows
up arrow
CIPAxisFaults (CD)
MotorOvercurrentFault
MotorCommutationFault
MotorOverspeedFLFault
MotorOverspeedULFault
MotorOvertemperatureFLFault
MotorOvertemperatureULFault
MotorThermalOverloadFLFault
MotorThermalOverloadULFault
MotorPhaseLossFault
InverterOvercurrentFault
InverterOvertemperatureFLFault
InverterOvertemperatureULFault
InverterThermalOverloadFLFault
InverterThermalOverloadULFault
ConverterOvercurrentFault
ConverterGroundCurrentFLFault
ConverterGroundCurrentULFault
ConverterOvertemperatureFLFault
ConverterOvertemperatureULFault
ConverterThermalOverloadFLFault
ConverterThermalOverloadULFault
ConverterACPowerLossFault
ConverterACSinglePhaseLossFault
ConverterACPhaseShortFault
ConverterPreChargeFault
BusRegulatorOvertemperatureFLFault
BusRegulatorOvertemperatureULFault
BusRegulatorThermalOverloadFLFault
BusRegulatorThermalOverloadULFault
BusRegulatorFault
BusModuleFault
BusUndervoltageFLFault
BusUndervoltageULFault
BusOvervoltageFLFault
BusOvervoltageULFault
BusPowerLossFault
BusPowerBlownFuseFault
BusPowerLeakageFault
BusPowerSharingFault
FeedbackSignalNoiseFLFault
FeedbackSignalNoiseULFault
FeedbackSignalLossFLFault
FeedbackSignalLossULFault
FeedbackDataLossFLFault
FeedbackDataLossULFault
FeedbackDeviceFault
SensorFault
BrakeSlipFault
HardwareOvertravelPositiveFault
HardwareOvertravelNegativeFault
ExcessivePositionErrorFault
ExcessiveVelocityErrorFault
OvertorqueLimitFault
UndertorqueLimitFault
ExcessiveBusVoltageErrorFault
AmbientTemperatureRiseFault
IllegalControlModeFault
EnableInputDeactivatedFault
ControllerInitiatedFault
ExternalInputFault
CIPAxisFaults2 (CD)
ACLineOvervoltageFLFault
ACLineOvervoltageULFault
ACLineUndervoltageFLFault
ACLineUndervoltageULFault
ACLineHighFrequencyFLFault
ACLineHighFrequencyULFault
ACLineLowFrequencyFLFault
ACLineLowFrequencyULFault
ACLineVoltageUnbalanceFault
ACLineCurrentUnbalanceFault
ACLineVoltageSagFault
ACLineFrequencyChangeFault
ACLineSyncLossFault
ACLineSyncFailureFault
InverterGroundCurrentFLFault
InverterGroundCurrentULFault
InverterOutputPhaseShortFault
AuxiliaryPowerSupplyFLFault
AuxiliaryPowerSupplyULFault
BusInputOvercurrentFLFault
BusInputOvercurrentULFault
CIPAxisFaultsRA (CD)
CommutationStartupFault
MotorVoltageMismatchFault
FeedbackFilterNoiseFault
FeedbackBatteryLossFault
FeedbackBatteryLowFault
FeedbackIncrementalCountErrorFault
ControlModuleOvertemperatureFLFault
ControlModuleOvertemperatureULFault
ConverterPreChargeOverloadFLFault
ConverterPreChargeOverloadULFault
ExcessiveCurrentFeedbackOffsetFault
RegenerativePowerSupplyFault
PWMFrequencyReducedFault
CurrentLimitReducedFault
TorqueProveFault
DecelOverrideFault
PreventativeMaintenanceFault
MotorTestFault
HardwareConfigurationFault
FirmwareChangeFault
ConverterPreChargeInputDeactivatedFault
DCCommonBusFault
RuntimeErrorFault
BackplaneCommunicationErrorFault
SafetyModuleCommunicationErrorFault
ACLineContactorFault
ACLineResonanceFLFault
ACLineResonanceULFault
TrackStopFault
LostMoverAssociationFault
UnassociatedMoverFault
PeripheralHardwareFLFault
PeripheralHardwareULFault
PeripheralOverTemperatureFLFault
PeripheralOverTemperatureULFault
PeripheralUnderTemperatureFLFault
PeripheralUnderTemperatureULFault
PeripheralCommunicationFLFault
PeripheralCommunicationULFault
AdapterCommunicationFLFault
AdapterCommunicationULFault
MechanicalBrakeOutputFault
ExcessiveMotorVoltageFeedbackOffsetFault
ACLinePhaseReversalFault
PhaseThermalImbalanceFault
DCBusVoltageImbalanceFault
PredictiveMaintenanceFault
ProductSpecificFault
ModuleSyncFault (S,SD, CD)
TimerEventFault (S,SD, CD)
ModuleConnFault (CD)
ConnFormatFault (CD)
LocalModeFault (CD)
CPUWatchdogFault (CD)
ClockJitterFault (CD)
CyclicReadFault (CD)
CyclicWriteFault (CD)
ClockSkewFault (CD)
ControlConnFault (CD)
ClockSyncFault (CD)
LogicWatchdogFault (CD)
DuplicateAddressFault (CD)
SystemConnectionFault (CD)
Entregue su opinión
¿Tiene dudas o comentarios acerca de esta documentación? Por favor deje su opinión aquí.
Normal