Create a Controller Project
To create a controller project, use the
Studio 5000 Logix Designer®
application.- Open the Logix Designer application and click New Project.
- Choose the controller catalog number, name the controller, and click Next.

- Define the properties of the controller, and click Finish:

Provide Feedback