Reset Button

You can reset the controllers or the safety partner with the reset button. The reset button is only read during a power-up or restart. If you press the reset button at another time, it has no effect.
For a safety controller, the Safety Locked status or safety signature does not prevent you from performing a controller reset. Because the application is cleared from the controller during a reset, the safety level of the controller is cleared also. When you download a safety project to the controller, the safety level is set to the level specified in the project.
A controller has two stages of reset:
  • A Stage 1 reset clears the application program and memory, but retains the IP address and all network settings. A stage 1 reset occurs only if the controller contains a user application.
  • A Stage 2 reset returns the controller to factory settings, including firmware, and clears all network settings. A stage 2 reset occurs only if the controller does not contain a user application, and the current controller firmware is not a 1.x version.
The Safety Partner reset returns the safety partner to out-of-box settings, including firmware.
IMPORTANT:
Because port enable/disable status is associated with the application program, the controller Ethernet port becomes enabled after a Stage 1 or Stage 2 reset.
WARNING: When you press the reset button while power is on, an Electric Arc can occur. This could cause an explosion in hazardous location installations. Be sure that power is removed or the area is nonhazardous before proceeding.
Controller Reset Button
This image shows the reset button on a ControlLogix controller.
Safety Partner Reset Button
This image shows the reset button on a GuardLogix controller safety partner.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal