Use
Who Active or
the Network Browser to Upload from the Controller

When you upload a project from the controller, it copies the project from the controller to the
Studio 5000 Logix Designer®
application.
You can use the features of the
Who Active or
Network Browser dialog box to upload from your controller after you have set the communication path.
IMPORTANT: With the Studio 5000 Logix Designer® application version 38.00.00 and later, RSWho/Who Active has changed to Network Browser.
Complete these steps to upload from the controller.
  1. After choosing the communication path, click Upload.
    This image shows how to upload a project in Logix Designer.
  2. On the Connected to Upload dialog box, verify the project to upload and click Upload.
    This image shows where to upload a project on the Connected to Upload dialog box in Logix Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal