Safety Project Configuration
NOTE:
The safety configuration descriptions only apply when you are using a
GuardLogix®
5580 controller.Safety projects require additional configuration after you create the project. These topics describe how to configure your controller.
For a safety-enabled controller, the programming software creates a safety task and a safety program. A main Ladder Diagram safety routine that is called MainRoutine is also created within the safety program.
A red bar under the icon distinguishes safety programs and routines from standard project components in the Controller Organizer.
Safety Components

Provide Feedback