Copy a Safety Network Number

If you must apply a Safety Network Number to other controllers, you can copy and paste the SNN.
To copy a Safety Network Number, complete the following steps.
  1. On the Online toolbar, click the Controller Properties icon.
  2. On the Controller Properties dialog box, click the Safety tab.
  3. Of the Safety tab, click the ellipse to the right of the Safety Network Number.
    This image shows where to click the ellipse for a SNN on the GuardLogix 5580 Properties dialog box in Logix Designer.
  4. On the Safety Network Number dialog box, click Copy and then OK.
    This image shows where to click to copy the SNN in Logix Designer.
  5. On the Controller Properties dialog box, click OK.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal