Set the Safety Level
The safety level declares the intent of the safety application. The safety level indicates whether the project is at safety level SIL 2/PLd or SIL 3/PLe.
- The safety level that is required for an application is based on a required risk assessment that you must perform.
- The safety level that is achieved is determined by conformance to Safety Integrity Level (SIL) and Performance Level (PL) requirements and safety application requirements.
You must specify the safety level:
- The default setting is SIL 2/PLd.
- You can only modify the setting offline, when the safety application is in the Unlocked state and no safety signature exists.
- For SIL 3/PLe, you must have a 1756-L8SP safety partner that is installed to the right of the primary controller. If you select SIL 3/PLe, a safety partner appears in the Controller Organizer I/O tree. If you change the value back to SIL 2/PLd, the safety partner disappears from the I/O tree.
Perform these tasks to set the safety level.
- On the Online toolbar, click the Controller Properties icon.
- On the Controller Properties dialog box, click the Safety tab.
- On the Safety tab, select the Safety Level.
- Click Apply and then OK.

Provide Feedback