Banner tab
How do I open the Banner tab?
In the expand the
Project Explorer
,Predefined Screens
folder, and double-click the Banner
item. The
System Banner
is included in each project by default. It is a rectangular banner that appears at the top of each screen and shortcut. The System Banner
contains a default set of items. There is only one
System Banner
per project. To omit the System Banner
from screens or shortcuts, change the properties of the screen or shortcut.The
Banner
is a predefined screen. When open, the Banner
appears in the Graphic Explorer
. Open the Banner
from the Project Explorer
to: - Add, move, or remove elements from theSystem Banner. Include only graphic elements to appear on every project screen.
- Change the appearance of the top of a screen by changing the fill color and height of theSystem Banner.
- Configure the properties of graphic elements on theSystem Bannerlike any other graphic element.
- Animate or create events for theSystem Banneror its graphic elements.
Provide Feedback