Add a graphic element to the System Banner
By default, the
System Banner
appears at the top of each screen and shortcut in a project. Customize the System Banner
by adding or deleting graphic elements. To add a graphic element to the System Banner
- In theProject Explorer, expand thePredefined Screensfolder.
- Double-click theBannerto open theSystem Banner.
- From theToolbox, drag the desired graphic element to theSystem Banner.
- If any portion of the graphic element is placed off the edge of the banner rectangle on theBannertab, that portion of the graphic element appears clipped in theSystem Banneron the HMI device.
- Placing a graphic element on top of the banner rectangle on an open screen rather than on theBannertab makes any portion of the graphic element that is on top of the rectangle on the screen not visible on the HMI device.
- Graphic elements with valid tag values placed off the banner rectangle do not appear on theSystem Banneron the HMI device. Graphic elements with invalid tag values are outlined in red. If a graphic element in error is placed near an edge or off theSystem Banner, an arrow with anErroricon
points in the direction of the graphic element. Tap the arrow to open the Error listfor the graphic element.TIP:Tips:- Using theGraphic Explorer, view and change graphic elements that are on theSystem Banner.
- Do not place a graphic element on top of theSystem Bannerat the top of an open screen. Place the graphic element on the banner rectangle on the openBannertab. Any portion of a graphic element placed on top of theSystem Banneron theScreentab rather than on theBannertab is not visible on the HMI device.
- After adding a graphic element to theSystem Banner, configure the element like any other graphic element, such as change properties and add animations and events.
- Adjust the height of theSystem Bannerto accommodate additional graphic elements. However, increasing the height of the banner decreases the amount of available screen space. Consider the size of the screen on the HMI device when adding graphic elements to theSystem Banner.
Provide Feedback