Remove the System Banner from a screen
The
System Banner
appears at the top of each screen in a project configured to show the System Banner
. Remove the System Banner
from any screen on which it is not to appear. Removing the System Banner
from a screen does not remove the System Banner
or its items from the project. To remove the System Banner from a screen
- In theProject Explorer, expand theUser-Defined Screensfolder.
- Select the screen.
- On thePropertiestab, expand theGeneralcategory.
- Clear theShowDefaultBannercheck box. TheSystem Bannerno longer appears at the top of the screen.TIP:Graphic elements placed at the top of the screen where theSystem Bannerwas located do not cover theSystem Banneron the HMI device if you later select theShowDefaultBannerbox again. For example, if you clear theShowDefaultBannerbox, place a rectangle at the top of the screen, and then select theShowDefaultBannerbox, the rectangle may cover theSystem BannerinView Designer. However, the rectangle does not cover theSystem Banneron the HMI device.
Provide Feedback