What is the System Banner?
The
System Banner
appears at the top of each screen configured to show the System Banner
, and each shortcut to which you have access. The System Banner
contains a default set of items. Security access to the System Banner
cannot be set for a particular role. You can remove the System Banner
from a screen or shortcut through the Properties
window for the selected screen or shortcut. You can change the height of the
System Banner
, but not the width. The System Banner
is always as wide as the screen. If you do not scale screens and change the HMI device type for your project, this affects the
System Banner
. For example, blank space appears to the right of the System Banner
when you configure the project for larger HMI device screens. Space to the right of the System Banner
is removed when you configure the project for smaller HMI device screens. When you do not scale screens and change project settings to a smaller HMI device, elements may appear clipped at the right end of the System Banner
on the HMI device. Provide Feedback