System Banner contents
By default, a
System Banner
appears at the top of each screen in a project. The System Banner
contains a default set of items:
Item | Description | |
![]() | Alarm Status Indicator opens the Alarm Summary screen on the HMI
device.
| |
![]() | ![]() | Automatic Diagnostics Indicator opens Automatic Diagnostics screen
on the HMI device. The button shows a notification with the number of active
diagnostics. The button returns to an outlined icon when no diagnostics are
active. |
![]() | Previous displays the previous screen in the navigation history on the HMI
device. | |
![]() | Next displays the next screen in the navigation history on the HMI device.
To navigate with Next requires displaying a previous screen first. | |
![]() | ![]() | Navigation displays the Navigation menu at the bottom of the screen
on the HMI device. Use the Navigation menu to display shortcuts and folder
contents. |
![]() | Log On logs on or off the project. The name of the logged on user appears
in the System Banner . The logged on user sees only the screens for which
the assigned user role has access. | |
![]() | General Diagnostics Status for the data log status and project event
errors. These icons appear depending on the status of data export and project
events.
A data log status icon only appears when a project contains a data log and there
are no project event errors.
| |
![]() | A Network Status icon appears only if there is an issue with network
communication. Select the icon to open the HMI Device Configuration Network
popup for details about the issue.
| |
![]() | A Controller Status icon appears only if there is an issue with any
controller in the project. Select the icon to open the Controllers General
popup for details about the issue.
| |
![]() | The current time and date of the HMI device. | |
Provide Feedback

Turns red and flashes when there are active alarms that are
unacknowledged. The numbered notification shows the number of unacknowledged
alarms.
Returns to a gray icon with a numbered notification showing the
number of unacknowledged alarms when all alarms return to normal but some
alarms are still unacknowledged.
Turns to red when there are active alarms and all of them are
acknowledged.