Change the background color of the System Banner

Change the background color of the
System Banner
that appears at the top of each screen in a project. Change the fill color of the banner to a different color, a gradient color, or a custom color.
To change the background color of the System Banner
  1. In the
    Project Explorer
    , expand the
    Predefined Screens
    folder.
  2. Select the
    Banner
    item or double-click it to open the
    System Banner
    .
  3. In the
    Properties
    window, click the
    Properties
    tab.
  4. Expand the
    Appearance
    category.
  5. In the
    FillColor
    box, select a color using one of the these methods:
    • Type the Hex value in the format #RRGGBB. R, G, and B are Hex digits from 0 through F and represent the color channel values for red, green, and blue. For example, #ffff00 produces yellow.
    • Select the arrow or color swatch to open the
      Color Picker
      , and select or create a color.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal