Work with instances of an Add-On Graphic
Work with instances of an Add-On Graphic in a project like any other graphic element. Resize, position, group, and copy and paste instances of an Add-On Graphic.
Rockwell Automation
recommends using no more than 500 elements on a screen. Each AOG instance adds the number of elements contained in that AOG toward the recommended limit of 500 elements. For example, assume there is an AOG defined that contains 10 elements. Now assume we instance that AOG 10 times on a screen. That accounts for 100 elements on the screen.Provide Feedback