Copy an instance of an Add-On Graphic within a project

Copy an instance of an Add-On Graphic to reuse the Add-On Graphic in the same project. Copying multiple instances of Add-On Graphics that are linked to different Add-On Graphic definitions is allowed. Copied instances of Add-On Graphics may be contained in groups.
When copying the instance of an Add-On Graphic within a project, the instance is linked to the existing definition of the Add-On Graphic.
To copy an instance of an Add-On Graphic within a project
  1. On the screen, right-click the Add-On Graphic instance and select
    Copy
    .
  2. Open the target screen.
  3. Right-click the screen canvas and select
    Paste
    . Another instance of the Add-On Graphic is created and copied to the screen.
    TIP:
    Tips:
    • Pasting an instance of an Add-On Graphic for which there is no definition is not allowed. Pasting an instance of an Add-On Graphic is not supported when deleting the definition of the Add-On Graphic before pasting the instance.
    • Copying an instance of an Add-On Graphic that is linked to an Add-On Graphic definition that contains an image, does ont create a new image asset in the
      Assets > Images
      folder in the
      Project Explorer
      .
Any changes to an instance of an Add-On Graphic do not affect any other instances of the Add-On Graphic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal