Change the properties of a graphic element

Change the attributes of a graphic element or Add-On Graphic, such as position and size, using the
Properties
tab in the
Properties
window.
To change the properties of a graphic element
  1. On the screen or in the
    Graphic Explorer
    , select the graphic element.
    • To select multiple elements, press and hold
      Ctrl
      while selecting each graphic element.
    • To select all of the graphic elements, press
      Ctrl+A.
  2. In the
    Properties
    window, select the
    Properties
    tab to display the properties for the selected graphic element
    TIP:
    Select multiple instances of Add-On Graphics to change the properties common to each instance instead of having to select and change the property values of each Add-On Graphic instance individually.
  3. Change any or all of the properties:
    • Type or select a value.
    • Bind the property to a data item.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal