Create a DeskLock System Restart button

Use the
Insert an ActiveX Control
dialog box to create a
DeskLock System Restart
button.
To create a DeskLock System Restart button
  1. From the
    Objects
    menu, select
    ActiveX Control
    .
  2. Drag the ActiveX tool to draw a rectangle the size you want the object to be.
  3. In the
    Insert an ActiveX Control
    dialog box, select
    DeskLock System Restart Button
    from the list of registered objects.
  4. Double-click the button to open its
    Properties
    dialog box.
  5. In the
    Properties
    dialog box, specify how the button looks, the action to be initiated by the button, and its tags or expressions.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal