Set up system restart settings (General tab)
The
DeskLock System Restart
button provides a way to shut down, or to shut down and restart, the operating system.To specify whether the button press will shut down or restart the operating system
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theGeneraltab.
- From the menu, select whether the button press will restart, or shut down the operating system.
- Select whether the system shutdown will force all applications running on the computer to close.
Provide Feedback