Set up connections for the DeskLock System Restart button (Connections tab)
Use the
Connections
tab to set up tags and expressions for the DeskLock System Restart
button.To set up tags and expressions for the DeskLock System Restart button
- In theGraphics Displayeditor, double-click the button to open itsPropertiesdialog box.
- Click theConnectionstab.
- Assign a tag or expression to these connections:
Provide Feedback